A perfect match:
igus & HARTING
for the perfect connection

Harnessed cables with HARTING plug-in connector

A Perfect Match - igus readycable: industrial cable harnessing of chainflex cables with HARTING industrial plug-in connectors. Whether harnessed control cables or individual made-to-measure harnessing with no minimum order quantity - the extensively tested chainflex cable quality in conjunction with the HARTING connector types Han 3A, 6B, 10B, 16B and 24B as a ready-to-connect readycable solution for industrial applications helps to save complex connector harnessing and guarantees safe components.
 

Monoblock or modular system

What is monoblock technology?

Only one insert is installed per connector housing. We offer these Harting plug-in connectors in housing sizes 6B, 10B, 16B and 24B.
The Harting plug-in connectors of the Han® EE series are designed for 500V contamination degree 3 when fully assembled. A modified contact arrangement allows use in the same degree of contamination for higher voltages up to 1,000V. When the plug-in connectors are fully equipped, a higher reference voltage is also possible, but with a lower degree of contamination. 

What does modular system mean?

Han-Modular® combines several Harting connector modules within one housing. It is possible to combine signals, power, data and even pneumatics all in one connector housing.  
The standard housing sizes remain the same and instead of a monoblock, various inserts can be combined within one housing. 
In addition, space requirements are reduced, as the number of housings is reduced and functionality is increased at the same time.

Would you also like to configure your modular system? 
Then talk to us. 
Request Han-Modular®
Harting monoblock
Harting Modular

Monoblock technology

... Try it ...

HARTING & igus: free sample
Go to free sample

Industrial plug-in connector by HARTING

What is special about it?

Good reasons for igus to trust in the partnership with HARTING when it comes to cable harnessing: in addition to the capability of integration into their own production, the following criteria were significant for choosing HARTING as supplier for modular plug-in connectors: 
 
  • Quality and innovation of the plug-in connectors
  • Reliable deliveries and competitiveness of the supplier
  • Variable cable harnessing based on Han-Modular® and all conventional installation sizes Han 3A, 6B, 10B, 16B and 24B
  • Clarity of design of HARTING rectangular connectors: simple assembly of all parts, such as connector housings, bolt and socket inserts or cable glands
Cable harnessing with HARTING connectors

Assemble igus cables with HARTING connectors

igus readycable & HARTING

What is typical of this special partnership?

igus readycable production can play to its strengths with HARTING as supplier and design-in partner of modular Han® industrial plug-in connectors .  Quality, lead time, productivity and also price are good reasons for industrial cable harnessing at igus. Combining this machine processing of the contacts in the inserts by HARTING with upstream machine cable processing, specialised harnessing areas and Kanban bearings leads to unrivalled flexibility of igus readycable:
  • Ready-to-connect directly from the cable manufacturer
  • Exactly in the desired length (cut with cm accuracy) 
  • No minimum order value or quantity
  • Ready to ship within 24hrs from stock 
  • Special forms of harnessing are part of our everyday business

Why should the product live up to its promises

"36-month chainflex cable guarantee and service life calculator based on 2 billion test cycles per year"

The chainflex cables used for readycable products are intensively tested in the company's own 3,800m² test laboratory, the largest in the industry. The ready-to-connect readycable cables guarantee a long service life thanks to extensive tests and quality inspections in the company's own laboratory, and more than 25 years of experience in the manufacturing and harnessing of cables.
 
igus is now the first German firm to have this promise validated for chainflex cables. In a complex certification process, the US "Underwriters Laboratories" institute confirmed the accuracy of the "igus® 36-month chainflex® cable guarantee and service life calculator based on two billion test cycles per year"promise. This makes the Cologne-based company the first in Europe to have the veracity of an advertising statement confirmed by a testing institution. In future, every chainflex cable that leaves the factory anywhere in the world will be identified by the UL marketing label with its unique number (B129699), referring to igus.
chainflex UL-verified marketing label

Module Connect

Module Connect - the interface made to measure

One ready-to -connect connector module instead of many individual connectors

The Module Connect is a new kind of plug-in connector for the connection of electric cables, fibre-optic cables and pneumatic hoses. It is characterised by a space-saving, low-profile housing and can be used wherever a large number of cables have to be connected in an installation space as small as possible.
 
This is a joint development of igus & HARTING, which makes use of the highly customisable Han-Modular plug-in connector by HARTING. All parts in the form of used modules, articulated frames and housings can be combined with each other as desired on a modular basis and be ordered for cable harnessing at igus as readycable. Back in 2018, igus gave the green light for the first sample projects.

More industrial plug-in connectors

High-performance plug-in connectors, signal plug-in connectors and several thousand connector components – igus provides a high level of availability with short delivery times.

Cables sold by the metre

Cables sold by the metre for moving applications in energy chains: chainflex meets all requirements for electromagnetic compatibility as well as the standards and guidelines such as UL, CSA, EAC and much more.

Ready-to-connect drive cables

Offering around 4,600 harnessed motor, servo, signal and encoder cables, igus is the world's No. 1 when it comes to harnessed cables for use in energy chains.  

Ready-to-install energy supply systems

Harnessed energy supply systems from a single source: save up to 80% of process costs with our igus readychain offers.  


Consulting

I look forward to answering your questions

Shipping and consultation

In person:

Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH