Torque-resistant cables for vertical order pickers of up to twelve meters

chainflex power and signal cables avoid corkscrews when supplying the lift frame.

Profile

  • What was required: Heavy-duty energy and signal cables using a movable lift frame with several guide rollers up to the cabin of an order picking machine
  • Requirements: Space-saving guidance of electrical and hydraulic cables, application in the deflection system for long cable lengths 
  • Product: chainflex cables
  • Field of application: Forklifts, tractors and order picking machines
  • Success for the customer: Long-lasting cable solution for sophisticated geometry of lift frame and guide roller

About vertical order pickers: The vertical order pickers of the EK-X series are very impressive in the broad range of products offered by Still - the Hamburg-based company is part of the Kion Group - which in turn is the world's second largest manufacturer of forklifts with a turnover of almost 4.5 billion euros (2013). Their job is to approach the pallets in the narrow aisles of a high-bay warehouse from which the driver removes individual boxes. The pickers reach picking heights of up to twelve metres and can be perfectly adapted to the individual application thanks to the modular design principle. The buyer can, for example, choose from different cabins, lifting masts, control panels and battery systems, and individually designed options are also implemented.
Still with chainflex

chainflex cables over rollers

Challenge

The deflection principle for cable guidance has already been used by Still for smaller order picking devices and has proven to be very successful. For the EK-X type series the lateral guide of the roller was improved slightly due to the greater cable lengths – and then the initial tests quickly showed that unfortunately, in this case, this solution did not work. Volker Haspel, who is responsible for electrical engineering at Kion Systems: "The cables that we used, twisted and looked like a corkscrew. Shortly afterwards they failed in the test. The testing of such cables is definitely a complex task. They execute relative motions in the lift frame and high dynamics occur when moving the order picker. Moreover, you have to take the tensile force that occurs here into account, which is different than the situation with energy chain cables". “

Solution

Tests in the laboratories of both companies showed: The special chainflex cable structure with cores wound in bundles also works very well on the rollers. Thereby the cores are first wound in bundles, which in turn are braided with a small pitch length around a core element. This core element is not used as a filler, rather it is designed as a strain relief element. In appearance the result is highly reminiscent of a steel rope. To additionally support this stable braiding construction a jacket is extruded under pressure to supplementally guide the wires in the longitudinal direction. All of these measures result in the fact that the forces occurring in the cable are minimized and the construction remains intact.
 
Also the special materials of the jacket and its workmanship are significant additional aids for durability. It was shown that the shape of the roller does not have an influence on service life. The decision was clear for the Still designers; the cable was defined as the standard for the lift frame of the EK-X.A chainflex cable with cores wound in bundles and TPE jacket is used which are between 4.50 and 16 metres long in the order pickers. There is no question that they are highly stressed. In many applications the devices are in continuous use, which means that the lift frame is always in motion. The chainflex cables move under these conditions just like they move in many thousands of energy chain applications. With this cable Still has found a solution for a task that arose through the changed geometry of lift frame and guide roller. The cable specialists at igus have also gained an insight: now they know that their cables are not only chain-suitable, but they have also proven to be effective in roller guides.
Go to the chainflex® overview

chainflex cores wound in bundles In the chainflex cables the cores are wound in bundles and were developed especially for use in energy chains. In bending processes they do not develop "corkscrews" and consequently they are chain-suitable without restriction.
still forklift with CF


Consulting

I look forward to answering your questions

Shipping and consultation

In person:

Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH