Examples of successful applications in the renewable energy industry

View success stories by energy type: ▶ Solar | ▶ Wind | ▶ Water

Solar

Reliable movement with igubal pillow block bearings in solar trackers

To ensure that solar unit daily tracking movement works perfectly, the company uses our robust igubal ESQM pillow block bearings - a "fit and forget" solution, since they are maintenance-free throughout their 25-year service life.
More about the application
Axiom Research Labs solar trackers
Axiom Research Labs solar trackers

Durable in any weather: iglidur P plain bearings in the PV tracker

Tracking systems from TecnoSun Solar Systems score highly in terms of cost efficiency thanks to their low installation height. iglidur P plain bearings are used in the traction ring. They can withstand all weathers, are insensitive to dirt and can easily withstand high loads caused by snow.
More about the application
PV tracking system from TecnoSun Solar Systems
PV tracking system from TecnoSun Solar Systems

Media-resistant plain and spherical bearings in the remotely controlled solar cleaning robot

The remote-controlled cleaner from TG hyLIFT removes fine dust, bird droppings and lichen from solar surfaces. Media-resistant iglidur P plain bearings are used in the wheels and self-aligning igubal fixed flange bearings in the rotating brush, which work without any problems with prolonged contact with water and cleaning agents.
More about the application
Solar plant cleaning robot from TG hyLIFT
Solar plant cleaning robot from TG hyLIFT

20 years of precisely mounted mirrors in solar steam system

iglidur plain bearings made of the material J UV ensure a permanently smooth operation in around 1,000 bearing points of the Fresnel collectors from Ecotherm. The material was specially developed for use in UV radiation.
More about the application
Solar steam system from Ecotherm
Solar steam system from Ecotherm

More cost-effective and more durable alternative to roller bearings in parabolic mirrors

The parabolic mirrors from Mithras Holding are equipped with durable special plastic plain bearings. Unlike rolling bearings, they do not require any maintenance due to the solid lubricants integrated in the material and are cheaper to manufacture.
More about the application
Parabolic trough system from Mithras Holding
Parabolic trough system from Mithras Holding

Wind

Top drive: Energy chains show themselves to be a reliable alternative to service loops on drilling rigs

The start-up WP Systems has developed a mobile maintenance platform for the rotors of wind turbines, which allows repair work in almost any weather and at any time of the day. Our flexible cables, energy chains and plain bearings are on board.
More about the application
Maintenance platform for wind turbines
Maintenance platform for wind turbines

Water

Safe energy supply in the point absorber even with high waves

The point absorbers from CorPower Ocean are lightweight, compact and cope well with storms thanks to the new "Wavespring Phase Control Technology". Two E4.1 series e-chains together with chainflex servo, power and control cables ensure safe energy supply within the buoy.
More about the application
Point absorber from CorPower Ocean
Point absorber from CorPower Ocean

Robust plain bearings for long service life of the wave energy converter

iglidur Z plain bearings are used in the WEC from Rotary Wave. They are extremely resilient, suitable for the harsh seawater environment and achieve significantly better results than sintered plain bearings with a bronze surface, for example.
More about the application
Wave energy converter from Rotary Wave
Bearing position in Rotary Wave's WEC

First plastic WEC to move reliably with plain bearings for underwater use

PolyGen's wave energy converter is the world's first WEC to be made predominantly of plastic. iglidur flanged bushings made of the material H370, specially developed for the wet area, were used on the axes of the flaps.
More about the application
PolyGen wave energy converter
PolyGen wave energy converter

Uninterruptible power transmission at the tidal turbine

The company Tocardo relies on our plastic E4/4 series energy chain to guide cables safely from the turbine to the converter in the switch cabinet and thus achieve the longest possible service life for the system. The chain is corrosion-resistant, easy to fit and quickly openable.
More about the application
Tocardo tidal turbine
Tidal turbine from Tocardo with e-chain

Tidal turbine moved safely in rough seas with e-chain and cables for movement

On the OpenHydro tidal turbine, the combination of our e-chain E4/4 with flexible chainflex motor and signal cables ensures a safe energy supply when the turbine moves 20 metres down. A metal chain was not suitable for the harsh conditions at sea.
More about the application
Tidal turbine from OpenHydro
Tidal turbine from OpenHydro

Saves space and maintenance costs: basic flizz system on the rake cleaner

The H-cleaner from Muhr uses a proven standard for the energy supply to the carriage: the basic flizz system. It moves the cables safely over 15 metres. Although well hidden, the energy chain is easily accessible for maintenance or when new cables need to be added.
More about the application
basic flizz and Schlossmühle hydroelectric power station
basic flizz system


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH