The pipe handler is used to move the drill pipe from a horizontal position from the catwalk to the vertical fingerboard, where it is finally stored for later use. Energy chains are also used here, allowing the pipe handler both to travel vertically and be positioned horizontally for precise storage of the drill pipe in the fingerboard.
It is especially important that the vertical routing of the heavy cables be safe on its long travel path. Plastic energy chains have an especially great advantage here, since they reduce the total weight hanging on the pipe handler thanks to their low dead weight.
Monday to Friday from 7 am - 8 pm.Saturdays from 8 am- 12 pm.
24h